High-pressure control chatters

Liquid-filled bellows multifies the damping orifice in the inlet connection.

Install the pressure control so that liquid cannot collect in the bellows element (see instruction). Eliminate cold air flow around the pressure control. Cold air can create condensate in the bellows element. Fit a damping orifice (code no. 060-1048) in the end of the control connection furthest away from the control.