रेफ्रिजरेशन सिस्टमची समस्यानिवारण करताना आवश्यक माहिती
Upper alarm limit Here you set when the alarm for high temperature is to start. The limit value is set in °C (absolute value). The limit value will be raised during night operation. The value is the same as the one set for night setback, but will only be raised if the value is positive.