Fampahalalana tena ilaina rehefa mikorontana ny rafitra fitahirizana vata fampangatsiahana
Alarm delay (short alarm delay on air temperature) If the upper or the lower alarm limit values are exceeded, a timer function will commence. The alarm will not become active until the set time delay has been passed. The time delay is set in minutes.