ຂໍ້ມູນທີ່ ຈຳ ເປັນເມື່ອແກ້ບັນຫາລະບົບຕູ້ເຢັນ
Time delay for cooling (long alarm delay) This time delay is used during start-up, during defrost, immediately after a defrost. There will be change-over to the normal time delay (A03) when the temperature has dropped below the set upper alarm limit. The time delay is set in minutes.